Driving LEDs: How to Choose the Right Power Supply
Contributed By Convergence Promotions LLC
2011-05-27
LEDs are fast replacing fluorescent light bulbs and incandescent light bulbs in many lighting applications. In the past these sources could be driven directly from the main voltage, but this is not possible with LEDs. This article looks at what an LED is, how to drive it, and how to choose the right power supply for this requirement.
What is an LED?
Like regular diodes, light emitting diodes (LEDs) are constructed using a semiconducting material which has been "doped" with impurities in order to create a P-N (positive-negative) junction. Current flows easily from the P-side (anode) to the N-side (cathode), but not in the other direction (see Figure 1).
When placed in a circuit supplied by an external power source, current flows, and charge carriers (electrons and holes) flow into this junction from the electrodes, which are at different voltages. The electrons and holes are separated by an energy difference known as a "band gap."

Figure 1: N- and P-type doping of an LED.
When an electron meets a hole, it falls across the band gap from the higher to the lower energy level, releasing the band gap energy as a photon of light with a frequency, and hence a color that corresponds to the band gap energy. This relationship can be expressed using the following equation:

| Where | Eg | = Band gap energy |
| h | = Planck's constant | |
| c | = Speed of light | |
| λ | = Wavelength |
Table 1 shows the wavelengths and band gap energies of a number of colored lights.
| Color | Wavelength (nm) | Band Gap Energy, E(eV) |
| Infrared | λ >760 | E<1.63 |
| Red | 610< λ <760 | 1.63 |
| Orange | 590< λ<610 | 2.03 |
| Yellow | 570< λ<590 | 2.10 |
| Green | 500< λ<570 | 2.18 |
| Blue | 450< λ<500 | 2.48 |
| Violet | 400< λ<450 | 2.76 |
| Ultraviolet | λ<400 | 3.1 |
LED manufacturers can "tune" the band gap energy and hence the wavelength of the light emitted. This is achieved by increasing or decreasing the level of impurities, e.g. controlling the composition of the semiconductor. Adding more impurities will lower the band gap energy, increasing the wavelength of the emitted light.
The band gap of an LED changes with varying temperature, and the extent of this change can be predicted using Varshni's parameters (empirically measured values that are used in order to calculate temperature dependent band gap energies). This relationship is described in the following equation:

| Where | Eg | = Band gap energy |
| T | = Temperature (K) | |
| α, β | = Varshni parameters |
Since both α and β are constants for a specified LED, as the temperature increases, the band gap energy of the LED slightly decreases. As seen previously, decreasing the band gap energy will increase the wavelength of emitted light and slightly change the color of the light emitted. This is referred to as temperature dependent spectral shift.
Performance characteristics of LEDs
The voltage–current relationship of LEDs is given by Shockley's diode equation:


| Where | I | = Diode forward current |
| Is | = Reverse bias saturation current | |
| VD | = Diode forward voltage | |
| n | = Diode ideality factor | |
| VT | = Thermal voltage | |
| k | = Boltzman's constant | |
| q | = Charge on an electron | |
| T | = Temperature |
Since n, k, q and Is are constant for a given LED at a fixed temperature T, the V-I curve of an LED can be plotted using this equation as shown in Figure 2:

Figure 2: LED current versus voltage (25°C).
Shockley's equation also tells us that the forward voltage of the LED is temperature dependent. For a fixed forward current, as the temperature increases, the forward voltage of the LED decreases. This is because the saturation current Is is also dependent on temperature and can be estimated using the following equation:

1. LEDs operate much more efficiently (they possess a much higher lum/W value) at lower current levels.
As an example, we can use the figures for Cree's XM-L high flux LEDs [1]. When driving the LED at 3 A (and at 25°C), it will emit 976 lumens. The power required to do so is 3 A * 3.34 V, or 10.02 W, resulting in an efficiency of 97.4 lm/W.

Figure 3: LED luminous flux versus current (25°C).

Figure 4: LED luminous flux versus temperature (3 A).
However, when the LED is driven at 1.5 A, it will emit 590 lumens. The power required is 1.5 A * 3.14 V, or 4.71 W, resulting in an efficiency of 125.3 lm/W, a significant improvement. This higher efficiency means that there is less waste heat generated by the LED (self-heating) at lower currents that can alter both the wavelength and intensity of the emitted light, as well as altering the forward voltage by raising the junction temperature.
2. As has already been mentioned, an increase in temperature will decrease the forward voltage (and power) needed to maintain a constant current. However, the lumen output will also fall, and by a greater scale. This means that that even though less power is required to maintain a constant current level, the lower lumen output will mean that the overall efficiency of the LED will fall.
Why do I need to use a driver for my LEDs?
Choosing the right supply is key to ensuring that you get the best performance from your LED. The long lifetimes of LEDs foster the perception that the weakest link is now the power supply. Excelsys has chosen design techniques, market leading components, and thermal management techniques in order to provide solutions for customers with lifetime matching figures. We also have incorporated a number of design features that fit in nicely with LED market requirements:
- IP67 rated, waterproof metal casing and will probably be potted
- LEDs are non-linear devices (If vs. Vf) with a forward voltage that is temperature dependent — that is, it needs to be controlled by regulating current
- LEDs are low voltage DC devices with forward voltage requirements. LEDs also require protection against damage
- Incandescent light bulbs are purely resistive loads, LEDs are not. Drivers are required to provide a power factor close to one over all line and load conditions
- High efficiency (driven by lumens per watt demanded by luminaire designers)
- High reliability
- Long lifetime (power supplies now perceived as the weakest link in the chain), needs to be in the tens of thousands of hours
- UL8750 approved
- Future designs will have the capability to communicate with the power supplies
We have stated that LEDs are current driven devices, so why do companies offer both Constant Current (CC) and Constant Voltage (CV) solutions for LED drivers?
The reason for this is to give the light fixture designers a number of options in optimizing their system. If many strings of LEDs are used in series, the most efficient way to drive them is to use a constant current power supply and connect the LEDs directly across the terminals of the power supply. However, if strings of LEDs are connected in parallel, there may be an issue in trying to match the current in all the strings. A possible alternative to this would be to place an external component or active circuit to control the current. This may result in a slightly less efficient overall number of lumens per watt, but it allows the user to have full flexibility in ensuring that an identical current flows though many LED strings in parallel.
What is the difference between CC mode and CV mode?
Figures 5, 6, and 7 show the characteristics of three distinct modes of operation of a power supply. On each plot the axes are the same.
The X axis shows the load increasing, and the Y axis shows the output voltage of the module. The blue line is the voltage and the green line is the output current.
You will note the performance of the Constant Voltage power supply shown in Figure 5. It shows, as the terminology suggests, a unit that delivers a constant voltage as the load increases. The load current rises as demanded by the system, and will continue to increase to a point where the power supply will go into current limit mode in order to prevent damage to the power train. In the Excelsys catalog, this is represented by the LDV and LXV product ranges. A lot of common voltage requirements, and some not so common voltages, are covered by these ranges.

Figure 5: Constant voltage: Excelsys LDV and LXV ranges.

Figure 6: Constant current: Excelsys LDC, LXC, and LXD ranges.

Figure 7: CC and CV mode: Excelsys LBD product range.
Figure 6 shows how a constant current driver will behave. As the load increases the output current will remain fixed, with the voltage decreasing accordingly. This is covered by the Excelsys LDC, LXC, and LXD product ranges.
The latest design from Excelsys takes the two modes of operation and combines them onto one design. From Figure 7, you can see how the unit will initially behave as a constant voltage unit. Once the load current max is reached, the control loop will then hold the supply current at a constant value and reduce the output voltage accordingly. This type of approach has many benefits to the end designer in that if chosen correctly, both CC and CV mode designs can be achievable with one supply.
We can see how each of these design modes can be used to implement a solution for different lighting applications.
Case Study 1:
- Application: advertising signage
- Three diodes in series per strip, with reverse bias protection diode and series limit resistor
- Current is controlled by

| — Where Vcc = supply voltage | ||
| — ΣVf = sum of forward voltages of LEDs | ||
| — R = series resistor | ||
- Each strip consumes approx 300 mA
- Customer required fixed 12 V output
- Solution provided with LDV100 series
- Or alternatively use the LDB60-12 V models. When used below a five ampere load, the unit operates in a constant voltage mode
- Application: high bay lighting
- LED configuration of nine LEDs in series
- Vf of each LED will vary from 8 V to 10 V
- Customer drives the LEDs with 700 mA
- Pout = 700 mA (Forward current) * 90 (Vf max of nine diodes in series) = Minimum of 63 watts
- Voltage range of 72 to 90 volts
- Solution provided by LXC75 700 mA part
- Alternatively, an LDB product can be used to limit the current to 700 mA
References
- "Cree XLamp XM-L LEDs Data Sheet," Cree.
Disclaimer: The opinions, beliefs, and viewpoints expressed by the various authors and/or forum participants on this website do not necessarily reflect the opinions, beliefs, and viewpoints of DigiKey or official policies of DigiKey.