Accelerate Small Display Integration with Plug-and-Play 3.5” IPS HDMI TFTs

By เคนตัน วิลลิสตัน

Contributed By DigiKey's North American Editors

Designers selecting displays for industrial controls, medical equipment, and other compact systems need to squeeze more information into smaller screens while improving legibility, ease of use, and reliability. At the same time, they need to lower costs while accelerating development.

With traditional options, it is challenging enough to find the right combination of size, resolution, brightness, and industrial performance. Then the problem becomes ease of integration. Small industrial displays are typically offered as panels or modules, but these require designers to expend considerable effort wrestling with low-level drivers, backlighting, and electromagnetic interference (EMI) mitigation.

This article briefly reviews the challenges designers face in developing compact systems. It then introduces 3.5", high-visibility plug-and-play displays from Newhaven Display and shows how they can be quickly integrated and deployed.

Rising demands for compact high-resolution displays

Historically, small-form-factor equipment could make do with low-resolution screens. With their limited functionality, these legacy systems needed little more than simple menus and basic indicators. However, modern equipment requires high-resolution displays that can present complex data with a polished user experience.

These changes have been driven by the introduction of features such as Internet of Things (IoT) connectivity and sophisticated analytics. Consider portable diagnostic tools and measurement equipment. These devices need to do more than just report readings. They must provide deep performance insights and give visual guidance when addressing issues.

Platform evolution also drives resolution requirements. As classic embedded RTOS environments give way to modern platforms such as Linux, Windows Embedded, and Raspberry Pi, designers face a practical constraint: modern operating systems expect display resolutions of at least 640 × 480, which traditional displays for small-form-factor equipment simply cannot deliver.

From a development perspective, higher resolutions make it practical to reuse user interface frameworks, widgets, and icon libraries originally developed for desktops, tablets, or embedded systems with larger displays. This reuse helps ensure consistent branding and behavior across product families while avoiding one-off, low-level GUI work.

Why traditional small displays complicate integration

To meet these demands, designers are moving away from the 320 × 240 resolution common in small displays toward crisp, responsive 640 × 480 thin-film-transistor (TFT) screens with technologies such as in-plane switching (IPS) for accurate color and wider viewing angles. This quadrupling of pixel count delivers a superior user interface but also introduces two interrelated challenges.

High-resolution displays under 5 in. are typically offered as bare panels accessed through interfaces such as 24-bit RGB, LVDS, or MIPI-DSI. To integrate these panels, designers must contend with high-speed circuit design, fussy cabling, and EMI from the high-frequency signals. Similarly, small displays often come with “just-the-basics” backlighting, leaving designers to source LED drivers and implement dimming controls.

On the software side, bare panels lack standardized discovery mechanisms. Designers must manually configure display timings and develop custom drivers for touch input and backlight control. This work demands specialized graphics and OS expertise that may not be core to the product team’s focus, and it complicates testing, manufacturing, and field service.

Simplifying small-display integration with HDMI and USB

The 3.5" IPS HDMI TFT displays (Figure 1) from Newhaven Display address these issues by integrating a 640 × 480 panel, a high-brightness backlight driver, EMI shielding, and optional capacitive touch into a complete display assembly. With a pixel density of 228 pixels per inch (PPI), these panels deliver the resolution needed for information-dense human-machine interfaces (HMIs) without the traditional hardware design headaches.

Image of Newhaven Display 3.5” IPS HDMI TFT displaysFigure 1: Shown are 3.5” IPS HDMI TFT displays that integrate a sharp 640 × 480 panel into a complete plug-and-play assembly. (Image source: Newhaven Display)

The HDMI video interface software streamlines system bring-up. From the host system’s perspective, the displays behave as standard HDMI monitors rather than as unknown bare panels that require custom timing tables. Like any standard HDMI monitor, the interface uses Extended Display Identification Data (EDID) to advertise a 640 × 480 mode, enabling automatic detection on Windows, Linux, and popular single-board computer (SBC) platforms such as Raspberry Pi. This removes the need for low-level graphics driver work and minimizes the risk of misconfigured resolutions.

The touch-enabled NHD-3.5-HDMI-HR-RSXP-CTU (Figure 2) extends the philosophy of standard interfaces to its projected capacitive (PCAP) touch input. Here, a Micro-USB connector provides both 5 V power and touch data for the capacitive variant. The touch controller appears as a standard USB Human Interface Device (USB-HID) under Windows and Linux, so the operating system installs its own drivers automatically, without requiring vendor-specific kernel modules.

Image of Newhaven Display NHD-3.5-HDMI-HR-RSXP-CTU with dimensions (click to enlarge)Figure 2: The NHD-3.5-HDMI-HR-RSXP-CTU integrates a sharp 640 × 480 panel into a complete display assembly with EMI shielding around the high-frequency components. (Image source: Newhaven Display, modified by author)

The modules also simplify the overall assembly process. With bare panels, designers face a multi-step integration: mounting the TFT glass in a custom frame, securing a separate driver board elsewhere in the enclosure, routing delicate ribbon cables between components, and finding space for discrete LED driver circuitry. The 3.5" IPS HDMI TFTs reduce this to a single assembly with four corner mounting holes.

The two-cable architecture (HDMI for video and Micro-USB for power and touch) replaces fragile flex circuits with standard cables, and the connectors are positioned along one edge of the printed circuit board (pc board) for straightforward routing. The integrated EMI shielding further reduces enclosure-level mitigation requirements.

Achieve sunlight readability with IPS technology

The displays' use of IPS delivers excellent optical performance relative to traditional twisted nematic (TN) or vertical alignment (VA) panels. IPS provides a wide 85° viewing angle in all directions and maintains consistent color and contrast across viewing positions. A typical luminance of 810 candela per square meter (cd/m²) for the capacitive model supports use in high-ambient-light environments, enabling clear visibility for handheld instruments, control panels, and other applications in outdoor and industrial environments.

The non-touch NHD-3.5-HDMI-HR-RSXP model (Figure 3) shares the same overall architecture, but omits the PCAP overlay. This enables a brighter display of 950 cd/m², providing even better sunlight readability for applications where input is handled through physical buttons or other external controls. Current consumption for the non-touch model is also slightly lower (460 milliamperes (mA) typical versus 490 mA). The same HDMI and USB connectivity is retained, with USB providing power only.

Image of Newhaven Display NHD-3.5-HDMI-HR-RSXP with dimensions (click to enlarge)Figure 3: The NHD-3.5-HDMI-HR-RSXP offers a pre-integrated 640 × 480 display with a bezel opening instead of capacitive touch. (Image source: Newhaven Display, modified by author)

Both models are specified for operating temperatures from -20°C to +70°C and storage from -30°C to +80°C. Validation testing includes thermal cycling, vibration, and electrostatic discharge to ±8 kV in air and ±4 kV in contact. These characteristics support deployment in industrial, transportation, and light outdoor environments without requiring designers to implement their own display-level qualification.

Getting a quick start with hardware and software setup

At the hardware level, integration is centered on three primary interfaces (Figure 4). An HDMI Type A connector provides the video input, while a USB Micro-B connector supplies 5 V and, for the capacitive model, carries the USB-HID touch data. A small terminal block exposes the backlight driver control pin, which accepts either a simple enable signal or a pulse width modulation waveform between 5 kHz and 100 kHz. Status LEDs indicate power, HDMI link detection, and touch activity on the capacitive version, assisting with bring-up and field troubleshooting.

Image of key features of Newhaven Display 3.5” IPS HDMI TFTsFigure 4: Key features of the 3.5” IPS HDMI TFTs include an HDMI (1) and USB Micro-B (2) interface, LED indicators for HDMI, DC power, and touch detection (3-5), and a backlight terminal block (6). (Image source: Newhaven Display)

In both Windows 10 and 11, the display is automatically detected as a generic HDMI monitor. The capacitive model enumerates as a USB-HID touch device as soon as the USB link is connected. No dedicated driver installation is required, and standard display settings and touch calibration tools can be used.

Linux-based systems typically use HDMI and EDID for automatic mode detection in a similar way. In most configurations, the module appears as a standard HDMI display, and the system selects the 640 × 480 mode automatically. For platforms such as Raspberry Pi, the user guide provides example configuration lines to force the desired mode and timing when necessary. Touch input on the capacitive variant is exposed via the standard Linux input subsystem as a USB-HID device, which simplifies integration with common graphical frameworks.

The integrated LED driver’s control pin allows backlight brightness to be adjusted without adding a separate driver circuit. A static logic level can be used for simple on/off control, while a pulse width modulation input allows brightness to be tuned for low-light environments or to reduce power draw during idle periods. This approach avoids the switching noise and layout complexity associated with discrete high-voltage LED driver designs on the main pc board.

Conclusion

Designers of small-form-factor equipment that need a display face many integration, cost, and time-to-market challenges that can be met by Newhaven Display’s 3.5" IPS HDMI TFT modules. These combine 640 × 480 resolution, sunlight-readable IPS optics, standard HDMI and USB-HID interfaces, an integrated backlight driver, EMI shielding, and industrial environmental specifications, all in a highly integrated, plug-and-play package.

DigiKey logo

Disclaimer: The opinions, beliefs, and viewpoints expressed by the various authors and/or forum participants on this website do not necessarily reflect the opinions, beliefs, and viewpoints of DigiKey or official policies of DigiKey.

About this author

Image of Kenton Williston

เคนตัน วิลลิสตัน

เคนตัน วิลลิสตัน สำเร็จการศึกษาระดับปริญญาตรีสาขาวิศวกรรมไฟฟ้าในปี 2000 และเริ่มอาชีพของเขาในฐานะนักวิเคราะห์เกณฑ์มาตรฐานโปรเซสเซอร์ ตั้งแต่นั้นมา เขาทำงานเป็นบรรณาธิการของกลุ่ม EE Times และช่วยเปิดตัวและเป็นผู้นำสิ่งพิมพ์และการประชุมหลายรายการที่เกี่ยวข้องกับอุตสาหกรรมอิเล็กทรอนิกส์

About this publisher

DigiKey's North American Editors