Quick Test Proves High-Quality USB Cables Make a Big Difference

Charging our mobile phone is a daily activity for most of us. Like me, you've probably got your USB cable plugged into a charger. I've got plenty of USB cables lying around. I think they multiply like tribbles. Every time I buy another rechargeable gadget it comes with a full-sized USB to a micro USB cable.

I've got an 800 mA charger at my desk with a high-quality USB cable, right next to my coffee cup. The micro USB has a right angle, like the 3021080-10 USB A male to USB micro cable from Qualtek Electronics. The inner conductors are 24 AWG power and ground, and 28 AWG twisted pair for data. The diameter of the outer jacket is 4.5 millimeters (mm).

One morning I had my usual desk charger cable on another assignment. My phone was at 55% so I pulled a cable from my tangled cable stash and put it to work charging my phone. An hour later had only gone from 55% to 65%. It took all afternoon to charge my phone!

Okay, time to do some experimenting. I found an app for my Android called “Ampere” that displays the battery current draw when unplugged, and the charging current when plugged in. I took my favorite heavy-duty USB cable and repurposed it to charging my phone again. The charging current shown was a healthy 720 milliamps (mA), almost the same as the rated capacity as the AC adapter (Figure 1).

Figure 1: High-quality USB cables with a good AC adapter provide a healthy charging current. The AC adapter has a rated 800 mA capacity. (Image source: Bill Giovino)

While it’s expected that charging current may fluctuate while the phone runs mysterious tasks in the background, the charging current never went below 560 mA.

The cheapo unbranded USB cable only gave me a lousy 50 mA charging current (Figure 2). The charging current never faltered from 50 mA. I also had connection problems with this cable when trying to use it to transfer data between my phone and my laptop.

Figure 2: Low-quality USB cables with the same 800 mA AC adapter provide a sad charging current that never goes above 50 mA. (Image source: Bill Giovino)

The unbranded cable measured at about 10 AWG seen with my handy gauge meter in Figure 3, which according to specifications is a 2.588 mm outer jacket. The inferior cable is extremely flexible, while the quality cable is much more rigid. The quality USB cable clearly has thicker wires compared to thinner, less expensive cable.

Figure 3: The low-quality, unbranded USB cable measures as 10 AWG, circled in red. The high-quality cable is clearly thicker. (Image source: Bill Giovino)

Most mobile phones can sense if they are connected to a high capacity charger and adjust the charging current, from full charge down to slow trickle charge. All my high-quality USB cables charge the same, but for the lessor quality cables, no two cables charged with the same current – they are inexpensive cables with inconsistent quality.

Quality, plus innovation: USB cable is reversible!

As anyone who has used these cables can tell you, the annoying bit can be plugging them into the phone. Murphy’s Law of USB cables states that when plugging the USB cable into the side or the back of your laptop for the first time, it never seats. We’ve all done it. You plug it in, it doesn’t fit. Flip the connector over, plug it in – it still doesn’t fit. It can take 3 or 4 flips to get it right.

There’s a solution. The UR050-003-24G reversible USB A male to USB micro cable from Tripp Lite is very easy to use. The USB A Male end can be plugged into a computer in either direction, without having to flip it (what a great idea!). It’s also a heavy-duty cable. I’m getting two of them.

It’s not worth the hassle of buying the cheapest cable online when a few extra dollars spent on quality cables can make life so much easier.

About this author

Image of Bill Giovino

Bill Giovino เป็นวิศวกรอิเล็กทรอนิกส์ที่จบการศึกษาระดับปริญญาตรีจากมหาวิทยาลัย Syracuse และเป็นหนึ่งในไม่กี่คนที่ประสบความสำเร็จจากวิศวกรออกแบบวิศวกรแอปพลิเคชันภาคสนามไปจนถึงการตลาดด้านเทคโนโลยี

เป็นเวลากว่า 25 ปีแล้วที่ Bill มีความสุขในการส่งเสริมเทคโนโลยีใหม่ต่อหน้าผู้ชมทั้งทางเทคนิคและทางเทคนิคสำหรับหลาย ๆ บริษัท รวมถึง STMicroelectronics, Intel และ Maxim Integrated ในขณะที่ STMicroelectronics Bill ช่วยเป็นหัวหอกในความสำเร็จในช่วงแรกของ บริษัท ในอุตสาหกรรมไมโครคอนโทรลเลอร์ ที่ Infineon Bill ได้จัดเตรียมการออกแบบไมโครคอนโทรลเลอร์ตัวแรกของบริษัทที่ชนะในยานยนต์ของสหรัฐอเมริกา ในฐานะที่ปรึกษาด้านการตลาดของ CPU Technologies ของบริษัท Bill ได้ช่วยให้หลายบริษัทเปลี่ยนผลิตภัณฑ์ที่มีประสิทธิภาพต่ำให้กลายเป็นเรื่องราวแห่งความสำเร็จ

Bill เป็นผู้ใช้ Internet of Things ในยุคแรก ๆ รวมถึงการวางสแต็ก TCP / IP เต็มรูปแบบครั้งแรกบนไมโครคอนโทรลเลอร์ Bill ทุ่มเทให้กับข้อความ “การขายผ่านการศึกษา” และความสำคัญที่เพิ่มขึ้นของการสื่อสารที่ชัดเจนและเป็นลายลักษณ์อักษรในการโปรโมตผลิตภัณฑ์ทางออนไลน์ เขาเป็นผู้ดูแล LinkedIn Semiconductor Sales & Marketing Group ยอดนิยมและพูด B2E ได้อย่างคล่องแคล่ว

More posts by Bill Giovino
 TechForum

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.

Visit TechForum