SPA® Family ofTVS Diodes ArraysHigh Performance ESD and Lightning Surge Protectors Designed for I/O Interfaces |
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Littelfuse® SPA® Family of TVS Diode ArraysLittelfuse SPA family of TVS diode array devices are designed to protect electronics from very fast and often damaging voltage transients, such as lightning and electrostatic discharge (ESD). They offer an ideal protection solution for analog and digital I/O interfaces for markets including consumer, telecommunications, industrial, medical, computing, etc. Electrostatic Discharge (ESD) is an electrical transient that poses a serious threat to electronic circuits. The most common cause is friction between two dissimilar materials, causing a buildup of electric charges on their surfaces. Typically, one of the surfaces is the human body, and it is not uncommon for this static charge to reach a potential as high as 15,000 volts. At 6,000 static volts, an ESD event will be painful to a person. Lower voltage discharges may go unnoticed, but can still cause catastrophic damage to electronic components and circuits. These robust diodes can safely absorb repetitive ESD strikes at the maximum level (Level 4) specified in the IEC 61000-4-2 international standard, without performance degradation.
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| Voltage | Current | Rise-Time | Duration | |
|---|---|---|---|---|
| Lighting | 25 kV | 20 kA | 10 μs | 1 ms |
| Switching | 600 V | 500 A | 50 μs | 500 ms |
| EMP | 1 kV | 10 A | 20 ns | 1 ms |
| ESD | 15 kV | 30 A | <1ns | 100 ns |
Why are Transients of Increasing Concern?
Component miniaturization has resulted in increased sensitivity to electrical stresses. Microprocessors for example, have structures and conductive paths which are unable to handle high currents from ESD transients. Such components operate at very low voltages, so voltage disturbances must be controlled to prevent device interruption and latent or catastrophic failures.
| Device Type | Vulnerability (volts) |
|---|---|
| VMOS | 38-1800 |
| MOSFET | 100-200 |
| GaAsFET | 100-300 |
| EPROM | 100 |
| JFET | 140-7000 |
| CMOS | 250-3000 |
| Schottky Diodes | 300-2500 |
| Bipolor Transistors | 380-7000 |
| SCR | 680-1000 |
Sensitive microprocessors are prevelant today in a wide range of devices. Everything from home appliances, such as dishwashers, to industrial controls and even toys use microprocessors to improve functionality and efficiency.
Most vehicles now also employ multiple electronic systems to control the engine, climate, braking and, in some cases, steering, traction and safety systems.
Many of the sub- or supporting components (such as electric motors or accessories) within appliances and automobiles present transient threats to the entire system.
Careful circuit design should not only factor environmental scenarios but also the potential effects of these related components. Table 2 below shows the vulnerability of various component technologies.
| Series Name | Schematic (Example) | ESD Level (Contact) | I/O Cap | vRWM | Lightning (tP=8/20μs) | Number of Channels | Package Options |
|---|---|---|---|---|---|---|---|
| General Purpose ESD Protection
Protection for human interfaces (keypads, buttons, switches, audio ports, etc) |
|||||||
| SP1043 | ![]() |
±12 kV | 8 pF | 6 V | 1 A | 1 | 01005 Flipchip |
| SP3145 | ±20 kV | 0.35 pF | 3.3 V | 1 A | 1 | 01005 Flipchip |
|
| SP1003 | ±25 kV | 30 pF (17 pF @ 2.5 V) | 5 V | 7 A | 1 | SOD882 | |
| SOD723 | |||||||
| SP1044 | ±30 kV | 3 0pF | 6 V | 3 A | 1 | 01005 Flipchip |
|
| SP1006 | ±30 kV | 25 pF (15 pF @2.5 V) | 6 V | 5 A | 1 | μDFN-2 | |
| SPHV Series* | ±30 kV | 25-60 pF | 12-36 V | 8 A | 1 | SOD882 | |
| SD Series | ±30 kV | 50-350 pF | 5-36 V | 30 A | 1 | SOD323 | |
| SP1007 | ![]() |
±8 kV | 5 pF (3.5 pF @ 5 V) | 6 V | 2 A | 1 |
0201 |
| Flipchip | |||||||
| SP1002 | ±8 kV | 6 pF (5 pF @ 2.5 V) | 6 V | 2 A | 1 | SC70-3 | |
| 2 | SC70-5 | ||||||
| SP24-01WTG-C-HV | ±10 kV | 10 pF | 36 V | 1.5 A | 1 | Flipchip | |
| SP1014 | ±12 kV | 6 pF | 5 V | 2 A | 1 | Flipchip | |
|
SP1021 |
±12 kV | 6 pF | 6 V | 2 A | 1 | 01005 Flipchip | |
| SP1008 | ±15 kV | 9 pF(6 pF @ 5 V) | 6 V | 2.5 A | 1 | 0201 | |
| Flipchip | |||||||
| SP24-01WTG-C-HV | ±18 kV | 13 pF | 24 V | 3 A | 1 | Flipchip | |
| SM24CANA* | ±24 kV | 11 pF | 24 V | 3 A | 2 | SOT23-3 | |
| SP1026 | ±30 kV | 1 5pF | 6 V | 5 A | 1 | μDFN-2 (0201) | |
| SP1020 | ±30 kV | 20 pF | 6 V | 5 A | 1 | 01005 Flipchip | |
| SP15-01WTG-C-HV | ±30 kV | 21 pF | 15 V | 5 A | 1 | Flipchip | |
| SP12-01WTG-C-HV | ±30 kV | 26 pF | 12 V | 8 A | 1 | Flipchip | |
| SP1013 | ±30 kV | 30 pF | 5 V | 8 A | 1 | Flipchip | |
| SP1005 | ±30 kV | 30 pF (23 pF @ 2.5 V) | 6 V | 10 A | 1 | 0201 | |
| SM24CANB* | ±30 kV | 30 pF | 24 V | 10 A | 2 | SOT23-3 | |
| SM712* | ±30 kV | 75 pF | -7 V to +12 V | 19 A | 2 | SOT23-3 | |
| SM Series* | ±30 kV | 400 pF | 5-36 V | 24 A | 2 | SOT23-3 | |
| SD-C Series | ±30 kV | 200 pF | 5-36 V | 30 A | 1 | SOD323 | |
| SP1004 |
(4 Channel Shown) |
±8 kV | 6 pF (5 pF @ 1.5 V) | 6 V | 2 A | 4 | SOT953 |
| SP1012 | ±15 kV | 6.5 pF | 5 V | 3 A | 5 | Flipchip | |
| SP1001 | ±15 kV | 12 pF (8 pF @ 2.5 V) | 5.5 V | 2 A | 2 | SC70-3 | |
| SOT553 | |||||||
| 4 | SC70-5 | ||||||
| SOT553 | |||||||
| 5 | SC70-6 | ||||||
| SOT563 | |||||||
| SOT963 | |||||||
| SP1011 | ±15 kV | 12 pF (7 pF @ 2.5 V) | 6 V | 2 A | 4 | μDFN-6 1.25x1.0mm |
|
| SP050xBA | ±30 kV | 50 pF (30 pF @ 2.5 V) | 5.5 V | N/A | 2 | SOT23-3 | |
| SC70-3 | |||||||
| 3 | SOT143 | ||||||
| 4 | SOT23-5 | ||||||
| SC70-5 | |||||||
| 5 | SOT23-6 | ||||||
| SC70-6 | |||||||
| 6 | MSOP-8 | ||||||
| SP1015 |
|
±20 kV | 5 pF | 5 V | 2 A | 4 | 0.95X0.55MM Flipchip |
| New SP1064 |
±15 kV | 8.5 pF | 60 V | 2 A | 4 | μDFN-10 2.5x1.0 mm |
|
| Series Name | Schematic (Example) | ESD Level (Contact) | I/O Cap | vRWM | Lightning (tP=8/20μs) | Number of Channels | Package Options |
| General Purpose ESD Protection (SCR Diode Arrays) | |||||||
| SP721 | ![]() |
±4 kV | 3 pF | 30V or (±15V) | 3 A | 6 | SOIC-8 |
| PDIP-8 | |||||||
| SP720 | ±4 kV | 3 pF | 30V or (±15V) | 3 A | 14 | SOIC-16 | |
| PDIP-16 | |||||||
| SP724 | ±8 kV | 3 pF | 20V or (±10V) | 3 A | 4 | SOT23-6 | |
| SP723 | ±8 kV | 5 pF | 30V or (±15V) | 7 A | 6 | SOIC-8 | |
| PDIP-8 | |||||||
| SP725 | ±8 kV | 5 pF | 30 V or (±15V) | 14 A | 4 | SOIC-8 | |
| Series Name | Schematic (Example) | ESD Level (Contact) | I/O Cap | vRWM | Lightning (tP=8/20μs) | Number of Channels | Package Options |
| Low Capacitance ESD Protection
Protection for data lines (USB, HDMI, eSata, etc) |
|||||||
| SESD |
|
±20 kV | 0.25 pF | 7 V | 2 A | 1 | 0201 DFN* |
| 0402 DFN* | |||||||
| ±22 kV | 0.30 pF | 7 V | 2.5 A | 1 | 0402 DFN | ||
| New SP3530 |
±22 kV | 0.30 pF | 7 V | 2.5 A | 1 | 0201 DFN* | |
| SOD882* | |||||||
| SP3021 | ![]() |
±8 kV | 0.50 pF | 5 V | 2 A | 1 | SOD882 |
| SP3118 | ±10 kV | 0.30 pF | 18 V | 2 A | 1 | 0201 Flipchip | |
| SOD882 | |||||||
| SP3130 | ±10 kV | 0.30 pF | 28 V | 2 A | 1 | 0201 Flipchip | |
| SOD882 | |||||||
| SP3031 | ±10 kV | 0.80 pF | 5 V | 2 A | 1 | SOD882 | |
| SP3022 | ±20 kV | 0.35 pF | 5.3 V | 3 A | 1 | 0201 Flipchip | |
| SOD882* | |||||||
| SESD | ±20 kV | 0.13 pF | ±7 V | 2 A | 1 | 0201 DFN* | |
| 0402 DFN* | |||||||
| ±22 kV | 0.15 pF | 7 V | 2.5 A | 1 | 0402 DFN | ||
| New SP3522 |
±22 kV | 0.15 pF | 7 V | 2.5 A | 1 | 0201 DFN* | |
| SOD882* | |||||||
| New SP3042 |
±30 kV | 0.35 pF | 5.3 V | 2 A | 1 | 01005 Flipchip |
|
| SP0502B* |
(4 Channel Shown) |
±15 kV | 1 pF | 5 V | 2 A | 2 | SOT523 |
| SESD | ±20 kV | 0.20 pF | 7 V | 2 A | 2 | 0402 DFN | |
| 4 | 0802 DFN | ||||||
| 4 | 1004 DFN* | ||||||
| 6 | 1103 DFN | ||||||
| ±22 kV | 0.30 pF | 7 V | 2.2 A | 2 | 0402 DFN | ||
| 4 | 1004 DFn | ||||||
| New SP3222-02ETG |
±30 kV | 0.90 pF | 3.3 V | 3 A | 2 | SOD883 | |
| SP1255* |
|
±12 kV | 0.50 pF
(1300 pF Pin 1) |
4 V
(12 V Pin 1) |
4 A
(100 A Pin 1) |
3 | μDFN-6 |
| SP3001 | ![]() |
±8 kV | 0.65 pF | 6 V | 2.5 A | 4 | SC70-6 |
| SP3003 | ±8 kV | 0.65 pF | 6 V | 2.5 A | 2 | SC70-5 | |
| SOT553 | |||||||
| μDFN-61.6x1.0mm | |||||||
| 4 | SC70-6 | ||||||
| SOT563 | |||||||
| 8 | MSOP-10 | ||||||
| SP3004 | ±12 kV | 0.85 pF | 6 V | 4 A | 4 | SOT563 | |
| SP0504SHTG | ±12 kV | 0.85 pF | 6 V | 4.5 A | 4 | SOT23-6 | |
| SP3002 | ±12 kV | 0.85 pF | 6 V | 4.5 A | 4 | SC70-6 | |
| SOT23-6 | |||||||
| μDFN-61.6x1.6mm | |||||||
| SP3014 | ±15 kV | 1.0 pF | 5 V | 8 A | 2 | μDFN-6L 1.65x1.05mm | |
| SP8142-04UTG | ±22 kV | 1.0 pF | 5 V | 2.5 A | 4 | μDFN-10 2.5X1.35mm | |
| SP0524PTUG | ![]() |
±12 kV | 0.50 pF | 5 V | 4 A | 4 | μDFN-10 2.5x1.0mm |
| SP0544TUTG | |||||||
| SP3012-4 | |||||||
| New SP3422-04UTG |
±22 kV / -10 kV | 0.20 pF | 5 V | 2 A | 4 | μDFN-5 | |
| SP8143-06UTG | ±22 kV | 1.0 pF | 5 V | 2.5 A | 6 | μDFN-16 | |
| SP3010 | ![]() |
±8 kV | 0.45 pF | 6 V | 3 A | 4 | μDFN-10 2.5x1.0mm |
| SP3011 | ![]() |
±8 kV | 0.40 pF | 6 V | 3 A | 6 | μDFN-14 3.5x1.35mm |
| SP3012-6 | ![]() |
±12 kV | 0.50 pF | 5 V | 4 A | 6 | μDFN-14 3.5x1.35mm |
| SP7538PUTG | ![]() |
±12 kV | 0.50 pF | 5 V | 4 A | 8 | μDFN-9 |
| New SP8008 |
±30 kV | 0.30 pF | 5 V | 4 A | 8 | μDFN-14 | |
| Series Name | Schematic (Example) | ESD Level (Contact) | I/O Cap | vRWM | Lightning (tP=8/20μs) | Number of Channels | Package Options |
| Lightning Surge Protection
Protection for broadband data and communication lines (Ethernet, xDSL, etc) |
|||||||
| SP1555 | ![]() |
±30 kV | 800 pF | 15 V | 120 A | 1 | μDFN - 6 1.8x2.0 mm |
| SP1255-01UTG* | ±30 kV | 1300 - 2500 pF | 13.5 V | 160 A | 1 | μDFN - 6 1.8x2.0 mm | |
| SP3312* | ![]() |
±30 kV | 1.3 pF | 3.3 V | 15 A | 4 | μDFN-8 |
| SP4022* |
Undirectional | FV=ffecc644
±30 kV | 1.3 pF | 12 V | 15 A | 1 | SOD323 |
| SP4023* | ±30 kV | 1.3 pF | 15 V | 12 A | 1 | SOD323 | |
| SP4024* | ±30 kV | 1.3 pF | 24 V | 7 A | 1 | SOD323 | |
| SP4022-C* |
Bidirectional |
±30 kV | 1.3 pF | 12 V | 15 A | 1 | SOD323 |
| SP4023-C* | ±30 kV | 1.3 pF | 15 V | 12 A | 1 | SOD323 | |
| SP4024-C* | ±30 kV | 1.3 pF | 24 V | 7 A | 1 | SOD323 | |
| SLVU2.8 | ![]() |
±30 kV | 2 pF | 2.8 V | 40 A | 1 | SOT23-3 |
| SLVU2.8 | |||||||
| SLVU2.8-8 | ![]() |
±30 kV | 2.6 pF | 2.8 V | 30 A | 8 | SOIC-8 |
| SP2502LBTG | ![]() |
±30 kV | 5 pF | 2.5 V | 75 A | 2 | SOIC-8 |
| SP4040 | |||||||
| SR05 | ±30 kV | 8 pF | 5 V | 25 A | 2 | SOT-143 | |
| LC03-3.3 | ±30 kV | 9 pF | 3.3 V | 150 A | 2 | SOIC-8 | |
| SP4042 | ±30 kV | 11 pF | 3.3 V | 95 A | 2 | μDFN-10 (2.6x2.6mm) | |
| SP03-3.3 | ±30 kV | 16 pF | 3.3 V | 150 A | 2 | SOIC-8 | |
| SP03-6 | ±30 kV | 16 pF | 6 V | 150 A | 2 | SOIC-8 | |
| SP4044* |
|
±30 kV | 1.5 pF | 2.8 V | 24 A | 4 | MSOP-10 |
| SP4045* | 3.3 V | ||||||
| SLVU2.8-4 | ![]() |
±30 kV | 2 pF | 2.8 V | 40 A | 4 | SOIC-8 |
| SRV05-4 | ![]() |
±20 kV | 2.4 pF | 6 V | 10 A | 4 | SOT23-6 |
| SP3050 | |||||||
| SP2504NUTG | ![]() |
±30 kV | 3.5 pF | 2.5 V | 20 A | 4 | μDFN-10 (2.6x2.6) |
| SP4061 | |||||||
| SP3304NUTG | ±30 kV | 3.5 pF | 3.3 V | 20 A | 4 | μDFN-10 (2.6x2.6) | |
| SP4062 | |||||||
| New SP2555NUTG |
±30 kV | 2.5 pF | 2.5 V | 45 A | 4 | μDFN-10 (3.0x2.0mm) |
|
| SP2574NUTG | ![]() |
±30 kV | 5.0 pf | 2.5 V | 40 A | 4 | μDFN-10 (3.0x2.0mm) |
| SRDA05 | ![]() |
±30 kV | 8 pF | 5 V | 30 A | 4 | SOIC-8 |
| SP4060 | ![]() |
±30 kV | 4.4 pF | 2.5 V | 20 A | 8 | MSOP10 |
| SP4065 | 3.3 V | ||||||
| Series Name | Schematic (Example) | ESD Level (Contact) | I/O Cap | vRWM | EMI Filter Attenuation | Number of Channels | Package Options |
| ESD and EMI Filter Devices -
Protection for mobile device display interfaces (mobile phones, navigation devices, etc) |
|||||||
| SP5001 |
(4 Channel Shown) |
±15 kV | 1.3 pF | 5 V | 30 dB @ 800 MHz | 4 | TDFN-10 2.5X2.0mm |
| SP5002 | ±15 kV | 1.3 pF | 5 V | 30 dB @ 800 MHz | 6 | TDFN-16 4.0X2.0mm | |
| SP5003 | ±15 kV | 1.3 pF | 5 V | 16 dB @ 900 MHz | 4 | TDFN-10 2.5X2.0mm | |
| SP6001 |
(4 Channel Shown) |
±30 kV | 24 pF (CDIODE=12 pF) | 6 V | ≥ -30 dB @ 1 GHz | 4 |
μDFN-8 1.7x1.35mm |
| 6 |
μDFN-12 2.5x1.35mm |
||||||
| 8 |
μDFN-16 3.3x1.35mm |
||||||
| SP6002 | ±30 kV | 30 pF (CDIODE=15 pF) | 6 V | ≥ -30 dB @ 1 GHz | 4 |
μDFN-8 1.7x1.35mm |
|
| 6 |
μDFN-12 2.5x1.35mm |
||||||
Note: * AEC-Q Automotive Qualified Part
To view a datasheet click here to visit our part search and choose the appropriate series.
TVS Diode Array (SPA® Family) Catalog
Littelfuse SPA Devices are designed to protect electronics from very fast and often damaging voltage transients, such as lightning and electrostatic discharge (ESD). They offer an ideal protection solution for I/O interfaces and digital and analog signal lines, in computer and consumer portable electronics markets.
Littelfuse SPA Devices are available in a range of packaging configurations including DIP, SOIC, MSOP, SOT23, SOT143, SC70, SOT5x3, SOT953, μDFN, SOD723, and flipchip. View catalog.
AEC-Q101 TVS And Diode Arrays Selection Guide
This selection guide focus’s around automotive applications and the products meeting the qualifications within the product categories of TVS Diode Arrays and TVS Diodes.
The Littelfuse SP4044 and SP4045 Series TVS (Transient Voltage Suppressor) Diode Arrays offer circuit designers overvoltage solutions for 10GbE or 1GbE interfaces in small form factor SMT (Surface Mount Technology) MSOP-10 packages. These components combine the advantages of low off-state capacitance load and low dynamic resistance with a robust surge rating.
Designers of today's electronic devices have demanded more functionality with greater flexibility and higher levels of user interaction. These circumstances have helped in driving the development of nanometer chipsets along with a multitude of user interfaces or ports. The confluence of these two has made electronic devices more susceptible to ESD and required the need for a more robust solution. View guide.
Application Note: Selecting an Appropriate ESD Device
Board designers today are confronted with a multitude of choices for ESD protection. Often the designer is constrained by certain limits such as the amount of parasitic capacitance his/her application can withstand or the required ESD level the board must pass without fail. More often than not, the constraints do not narrow down the available number of ESD devices to a manageable list. This white paper will provide guidance to the designer that will help him/her in choosing an ESD device that will give the best chance of a successful first pass design. View application note.
Application Note: Tips for Enhancing ESD Protection
In this white paper we'll address various techniques a board designer can employ to help him/her attain the ESD level required for their design should the chosen ESD protection devices fail in-system ESD testing. View application note.
Application Note: USB3.0 Port ESD Circuit Protection
This article explains the issues in greater detail and shows USB3.0 eye diagram test results to prove why the right kind of silicon protection array is the best technology for protecting USB 3.0 applications against ESD. View application note.
Application Note: Ethernet Port Lightning, ESD and EFT Protection
Understanding the nature and "directionality" of the events listed above will help guide the designer in how to best protect an Ethernet port, and more importantly, how the device's pin connections will affect system performance. View application note.


High Performance Transient Voltage Protection With Devices That Meet the Latest High Bandwidth Requirements