CircuitPython LED Animations
2020-08-11 | By Adafruit Industries
License: See Original Project
Courtesy of Adafruit
Guide by Kattni Rembor
Overview
One of the first things many people do with CircuitPython is blink an LED. We even consider it our version of "Hello, world!" It's fairly simple code with the little red LED - set the LED to True, wait for the desired-on period, and set it to False for the desired off period. It gets a little more complicated with NeoPixels or DotStars - you have to set the LED to a color, wait, and then set the color to 0 to turn it off. Regardless, blinking is pretty easy. But what if you want to do more?
Creating a beautiful animated display on RGB LEDs, like NeoPixels and DotStars, is simple using the Adafruit CircuitPython LED Animations helper library. This library enables you to display a number of animations including comet, theatre chase, pulse, blink, color cycle, rainbow, sparkle, and more.
This library also includes pixel mapping and animation group helpers. The pixel mapping helper allows you to work with strips of LEDs arranged in a grid or other shape to display animations across the grid or shape horizontally and vertically. It also allows you to combine multiple sets of LEDs, e.g. two matrices, and treat them as one for animation purposes. The animation group helper allows you to keep multiple animations synchronized, or to display two separate animations on two separate pixel objects, e.g. two separate strips.
This guide will walk you through the key features of each animation, such as timing and other animation-specific customizations. It will cover the basics of pixel mapping to show you how to easily treat LEDs in a strip or series of strips as a grid to display animations, as well as the basics of animation groups to keep multiple animations in sync or display multiple animations across multiple sets of pixels.
Before we get animating, the first thing we'll do is look at what the basic import and setup looks like with the CircuitPython LED Animation library. Let's go!
Import and Setup
The LED Animation library is designed to make displaying LED animations super simple. The first thing you need to do is import the necessary modules from the LED Animation library and create your initial pixel object. Each animation is a separate module to ensure you only import exactly what you need.
CircuitPython LED Animation Library
To get the necessary libraries for this guide, download the latest CircuitPython library bundle from circuitpython.org.
Download the latest CircuitPython library bundle
Open the downloaded zip and find the following folder and file within the lib folder:
- adafruit_led_animation
- neopixel.mpy
Drag this folder and file to the lib folder on your CIRCUITPY drive.
Import and Setup
The rest of the guide will reference this page. When you are introduced to each animation, the code snippet will not include the entire setup found below. It is assumed that you have included the rest of the import and setup necessary to make the code run. If you find an example is not working, make sure you've included the entire import and setup found on this page.
An example of import and setup for the NeoPixel FeatherWing is as follows:
Download: file
import board
import neopixel
from adafruit_led_animation.animation.solid import Solid
from adafruit_led_animation.color import RED
pixel_pin = board.D6
pixel_num = 32
pixels = neopixel.NeoPixel(pixel_pin, pixel_num, brightness=0.2, auto_write=False)
First you import board and neopixel. Next, you import the Solid module and the color RED.
Next you identify the pin to which you've connected to your NeoPixels, board.D6 in this case, and the number of pixels connected, 32. This example uses the NeoPixel FeatherWing. If you're using some other NeoPixel form factor, you would change these variables to match the pin you chose and the number of pixels you connected.
Finally, you create the pixel object.
This guide will use NeoPixels for all the examples, but the LED Animation library works equally well with DotStar LEDs. If you are using DotStars, your import and setup will differ.
For example:
Download: file
import board
import adafruit_dotstar
from adafruit_led_animation.animation.solid import Solid
from adafruit_led_animation.color import RED
clock_pin = board.D12
data_pin = board.D11
pixel_num = 144
pixels = adafruit_dotstar.DotStar(clock_pin, data_pin, num_pixels, brightness=0.2,
auto_write=False)
This example imports the necessary modules and assigns the appropriate pins and number of pixels to use 144 DotStar LEDs connected to D12 and D11.
These are very basic examples of what your import and setup may look like. It will likely end up far more complicated than that as you begin to work with multiple animations and so on. Regardless, this gives you an idea of what to expect. Now it's time to start animating!
Basic Animations
The CircuitPython LED Animation library provides many animations. This section will cover the basic animations: solid, blink, colorcycle, chase, comet, and pulse. Most of these animations are displayed in a single color, with colorcycle cycling through a list of colors. Each animation has features you can adjust. We'll show the basics of using the animations and look at the specific features for each one. Let's get animating!
Most animations will run individually on the SAMD21 (M0) microcontroller boards, but some combinations of animations and the most complex animations will not. If you're interested in running all the animations, or many animations together, consider using at least a SAMD51 (M4) microcontroller.
Solid
Solid is the simplest of all the animations. It displays a single color. While this is easy enough to do alone without the LED Animation library, you may want to include a solid color in a series of animations, so we made it available.
First you import the Solid module and a color for it. See Import and Setup for the rest of the necessary imports and pixel object creation.
Download: file
from adafruit_led_animation.animation.solid import Solid
from adafruit_led_animation.color import PINK
Next, you create the Solid animation. Solid requires two arguments:
- pixel_object: The pixel object, e.g. pixels.
- color: The color to display, e.g. PINK. Can also be a color tuple, e.g. (255, 0, 0), or a hex color value, e.g. 0xFF0000.
Download: file
solid = Solid(pixels, color=PINK)
Then you need to display the animation.
Download: file
while True:
solid.animate()
That's all there is to displaying a solid color using the LED Animation library! Let's take a look at the next animation.
Blink
The blink animation flashes a single color on and off at a specified speed.
First, you import the Blink module and a color for it. See Import and Setup for the rest of the necessary imports and pixel object creation.
Download: file
from adafruit_led_animation.animation.blink import Blink
from adafruit_led_animation.color import JADE
Next you create the Blink animation. Blink requires three arguments:
- pixel_object: The pixel object, e.g. pixels.
- speed: The speed of the blinking in seconds, e.g. 0.5.
- color: The color to display, e.g. JADE. Can also be a color tuple, e.g. (255, 0, 0), or a hex color value, e.g. 0xFF0000.
Once created, you display the animation.
Download: file
blink = Blink(pixels, speed=0.5, color=JADE)
while True:
blink.animate()
That's all there is to blinking a color on and off using the LED Animation library! Let's take a look at the next animation.
ColorCycle
The ColorCycle animation allows you to provide a list of colors to cycle through at a specified speed.
First you import the ColorCycle module and one or more colors for it. See Import and Setup for the rest of the necessary imports and pixel object creation.
Download: file
from adafruit_led_animation.animation.colorcycle import ColorCycle
from adafruit_led_animation.color import MAGENTA, ORANGE, TEAL
Next you create the ColorCycle animation. ColorCycle requires two arguments and has an optional third. You'll likely want to specify the third, but the animation will run without specifying it.
Required:
- pixel_object: The pixel object, e.g. pixels.
- speed: The speed of color cycle in seconds, e.g. 0.5.
Optional:
- colors: The list of colors to display, e.g. [MAGENTA, ORANGE, TEAL]. This must be a list! Lists are one or more items in []. If no colors are provided, it defaults to cycling through rainbow colors. Can also be a list of color tuples, e.g. (255, 0, 0), or a list of hex color values, e.g. 0xFF0000.
Once created, you display the animation.
Download: file
colorcycle = ColorCycle(pixels, 0.5, colors=[MAGENTA, ORANGE, TEAL])
while True:
colorcycle.animate()
That's all there is to cycling through a list of colors using the LED Animation library! Let's take a look at the next animation.
Chase
This is a theatre marquee type chase animation, with definable length of lit LEDs and dark gap between lit LEDs.
First you import the Chase module and a color for it. See Import and Setup for the rest of the necessary imports and pixel object creation.
Download: file
from adafruit_led_animation.animation.chase import Chase
from adafruit_led_animation.color import WHITE
Next you create the Chase animation. Chase requires three arguments and has an optional three more. This animation will run without the optional arguments, but you'll likely want to specify size and spacing as well.
Required:
- pixel_object: The pixel object, e.g. pixels.
- speed: The speed of the chase movement in seconds, e.g. 0.1.
- color: The color to display, e.g. WHITE. Can also be a color tuple, e.g. (255, 0, 0), or a hex color value, e.g. 0xFF0000.
Optional:
- size: The number of pixels to turn on in a row, e.g. 3. Defaults to 2 if no size is provided.
- spacing: The number of pixels to turn off in a row, e.g. 6. Defaults to 3 if no size is provided.
- reverse: Optionally reverses the movement of the animation. Set to True to enable. Defaults to False.
Once created, you display the animation.
Download: file
chase = Chase(pixels, speed=0.1, color=WHITE, size=3, spacing=6)
while True:
chase.animate()
That's all there is to creating your own theatre chase animation using the LED Animation library! Let's take a look at the next animation.
Comet
This animation creates a comet of a specified speed, with a dimming tail of specified length.
First you import the Comet module and a color for it. See Import and Setup for the rest of the necessary imports and pixel object creation.
Download: file
from adafruit_led_animation.animation.comet import Comet
from adafruit_led_animation.color import PURPLE
Next you create the Comet animation. Comet requires three arguments and has an optional three more. You'll likely want to specify at least tail_length.
Required:
- pixel_object: The pixel object, e.g. pixels.
- speed: The speed of the comet in seconds, e.g. 0.1.
- color: The color to display, e.g. PURPLE. Can also be a color tuple, e.g. (255, 0, 0), or a hex color value, e.g. 0xFF0000.
Optional:
- tail_length: The length of the comet in pixels. Defaults to 25% of the length of the pixel_object if no length is provided. Automatically compensates for a minimum length of 2 and a maximum of the length of the pixel_object.
- reverse: Optionally reverses the movement of the animation. Set to True to enable. Defaults to False.
- bounce: Optionally "bounces" the comet along the strip by displaying it from the beginning of the strip to the end, and then reversing the movement once it reaches the end of the strip. Set to True to enable. Defaults to False.
Once created, you display the animation.
Download: file
comet = Comet(pixels, speed=0.01, color=PURPLE, tail_length=10, bounce=True)
while True:
comet.animate()
That's all there is to displaying a comet using the LED Animation library! Let's take a look at the next animation.
Pulse
This animation pulses all of the LEDs simultaneously a single color at a specified speed.
First you import the Pulse module and a color for it. See Import and Setup for the rest of the necessary imports and pixel object creation.
Download: file
from adafruit_led_animation.animation.pulse import Pulse
from adafruit_led_animation.color import AMBER
Next you create the Pulse animation. Pulse requires three arguments and has an optional fourth.
Required:
- pixel_object: The pixel object, e.g. pixels.
- speed: The speed of the pulse in seconds, e.g. 0.1.
- color: The color to display, e.g. AMBER. Can also be a color tuple, e.g. (255, 0, 0), or a hex color value, e.g. 0xFF0000.
Optional:
- period: The number of seconds over which to pulse the LEDs. Defaults to 5 if no period is provided.
Once created, you display the animation.
Download: file
pulse = Pulse(pixels, speed=0.1, color=AMBER, period=3)
while True:
pulse.animate()
That's all there is to pulsing a single color using the LED Animation library!
Next up, we'll look at running multiple animations in a sequence. Let's go!
Full Example Code
This is the simpletest example from the LED Animation library.
Download: Project Zip or led_animation_simpletest.py | View on Github
"""
This simpletest example displays the Blink animation.
For NeoPixel FeatherWing. Update pixel_pin and pixel_num to match your wiring if using
a different form of NeoPixels.
"""
import board
import neopixel
from adafruit_led_animation.animation.blink import Blink
from adafruit_led_animation.color import RED
# Update to match the pin connected to your NeoPixels
pixel_pin = board.D6
# Update to match the number of NeoPixels you have connected
pixel_num = 32
pixels = neopixel.NeoPixel(pixel_pin, pixel_num, brightness=0.5, auto_write=False)
blink = Blink(pixels, speed=0.5, color=RED)
while True:
blink.animate()
This is an example that runs all of the basic animations in a sequence.
Download: Project Zip or led_animation_basic_animations.py | View on Github
"""
This example displays the basic animations in sequence, at a five second interval.
For NeoPixel FeatherWing. Update pixel_pin and pixel_num to match your wiring if using
a different form of NeoPixels.
This example may not work on SAMD21 (M0) boards.
"""
import board
import neopixel
from adafruit_led_animation.animation.solid import Solid
from adafruit_led_animation.animation.colorcycle import ColorCycle
from adafruit_led_animation.animation.blink import Blink
from adafruit_led_animation.animation.comet import Comet
from adafruit_led_animation.animation.chase import Chase
from adafruit_led_animation.animation.pulse import Pulse
from adafruit_led_animation.sequence import AnimationSequence
from adafruit_led_animation.color import (
PURPLE,
WHITE,
AMBER,
JADE,
TEAL,
PINK,
MAGENTA,
ORANGE,
)
# Update to match the pin connected to your NeoPixels
pixel_pin = board.D6
# Update to match the number of NeoPixels you have connected
pixel_num = 32
pixels = neopixel.NeoPixel(pixel_pin, pixel_num, brightness=0.5, auto_write=False)
solid = Solid(pixels, color=PINK)
blink = Blink(pixels, speed=0.5, color=JADE)
colorcycle = ColorCycle(pixels, speed=0.4, colors=[MAGENTA, ORANGE, TEAL])
chase = Chase(pixels, speed=0.1, color=WHITE, size=3, spacing=6)
comet = Comet(pixels, speed=0.01, color=PURPLE, tail_length=10, bounce=True)
pulse = Pulse(pixels, speed=0.1, color=AMBER, period=3)
animations = AnimationSequence(
solid, blink, colorcycle, chase, comet, pulse, advance_interval=5, auto_clear=True,
)
while True:
animations.animate()
Animation Sequence
The LED Animation library makes displaying animations on LEDs super simple. You've gone through the basic animations and how to use each of them individually. What if you want to run multiple animations in sequence? The LED Animation library has you covered with AnimationSequence.
AnimationSequence allows you to display multiple animations in a sequence, with a definable interval and a few other customization options including clearing the pixels between animations and displaying them in a random order.
To use it, you'll want to include the following in your imports.
Download: file
from adafruit_led_animation.sequence import AnimationSequence
The rest of the imports and setup is the same, however, you'll want to include multiple animations this time. This example for the NeoPixel FeatherWing includes blink, comet, and chase. You'll create the pixel object and the animations the same way you did in the previous sections.
Download: file
import board
import neopixel
from adafruit_led_animation.animation.blink import Blink
from adafruit_led_animation.animation.comet import Comet
from adafruit_led_animation.animation.chase import Chase
from adafruit_led_animation.sequence import AnimationSequence
from adafruit_led_animation.color import PURPLE, AMBER, JADE
pixel_pin = board.D6
pixel_num = 32
pixels = neopixel.NeoPixel(pixel_pin, pixel_num, brightness=0.2, auto_write=False)
blink = Blink(pixels, speed=0.5, color=JADE)
comet = Comet(pixels, speed=0.01, color=PURPLE, tail_length=10, bounce=True)
chase = Chase(pixels, speed=0.1, size=3, spacing=6, color=AMBER)
Next, you'll create the AnimationSequence object. AnimationSequence takes up to six arguments, but you're most commonly going to use a combination these four:
- members: The animation objects or groups, e.g. comet, blink, chase.
- advance_interval: Time in seconds between animations if cycling automatically, e.g. 5. Defaults to None - it will not advance if an interval is not provided.
- auto_clear: Clear the pixels between animations. Set to True to enable. Defaults to False.
- random_order: Activate the animations in a random order. Set to True to enable. Defaults to False.
Check out the API documentation for information on the other two.
Download: file
animations = AnimationSequence(
comet, blink, chase, advance_interval=5, auto_clear=True, random_order=True
)
Finally, you'll display the animations.
Download: file
while True:
animations.animate()
Now you can display multiple animations in a sequence! Now we'll take a look at some more animations. Next up: rainbows!
Full Example Code
This example displays three animations in a sequence, at a 5 second interval, and in a random order.
Download: Project Zip or led_animation_sequence.py | View on Github
"""
This example uses AnimationsSequence to display multiple animations in sequence, at a five second
interval.
For NeoPixel FeatherWing. Update pixel_pin and pixel_num to match your wiring if using
a different form of NeoPixels.
"""
import board
import neopixel
from adafruit_led_animation.animation.blink import Blink
from adafruit_led_animation.animation.comet import Comet
from adafruit_led_animation.animation.chase import Chase
from adafruit_led_animation.sequence import AnimationSequence
from adafruit_led_animation.color import PURPLE, AMBER, JADE
# Update to match the pin connected to your NeoPixels
pixel_pin = board.D6
# Update to match the number of NeoPixels you have connected
pixel_num = 32
pixels = neopixel.NeoPixel(pixel_pin, pixel_num, brightness=0.5, auto_write=False)
blink = Blink(pixels, speed=0.5, color=JADE)
comet = Comet(pixels, speed=0.01, color=PURPLE, tail_length=10, bounce=True)
chase = Chase(pixels, speed=0.1, size=3, spacing=6, color=AMBER)
animations = AnimationSequence(blink, comet, chase, advance_interval=3, auto_clear=True)
while True:
animations.animate()
Rainbows
The CircuitPython LED Animation library includes a series of rainbow animations: rainbow, rainbowchase, rainbowcomet, and rainbowsparkle. This section will cover these animations and the available customizations for each of them. Let's make some rainbows!
Most animations will run individually on the SAMD21 (M0) microcontroller boards, but some combinations of animations and the most complex animations will not. If you're interested in running all the animations, or many animations together, consider using at least a SAMD51 (M4) microcontroller.
Rainbow
This animation displays a shifting rainbow across all the pixels with a number of customization options.
First, you import the Rainbow module. See Import and Setup for the rest of the necessary imports and pixel object creation.
Download: file
from adafruit_led_animation.animation.rainbow import Rainbow
Next you create the Rainbow animation. Rainbow requires two arguments and has an optional three more.
Required:
- pixel_object: The pixel object, e.g. pixels.
- speed: The refresh rate of the rainbow in seconds, e.g. 0.1.
Optional:
- period: The period over which to cycle the rainbow in seconds, e.g. 2. Defaults to 5 if no period is provided.
- step: The steps to take through the colorwheel (0-255). A step of 1 means cycling through the entire colorwheel, a step of 2 means it cycles through every other possible value. Defaults to 1 if no step is provided.
- precompute_rainbow: Precompute the rainbow which increases its speed but uses more memory. Set to False to disable if you are running into memory limitations. Defaults to True.
Once created, you display the animation.
Download: file
rainbow = Rainbow(pixels, speed=0.1, period=2)
while True:
rainbow.animate()
That's all there is to displaying a rainbow using the LED Animation library! Let's take a look at the next animation.
RainbowChase
This is a rainbow version of the theatre marquee type chase animation, with definable length of lit LEDs and the dark gap between lit LEDs.
First, you import the RainbowChase module. See Import and Setup for the rest of the necessary imports and pixel object creation.
Download: file
from adafruit_led_animation.animation.rainbowchase import RainbowChase
Next you create the RainbowChase animation. RainbowChase requires two arguments and has an optional five more. You'll likely want to at least specify size and spacing.
Required:
- pixel_object: The pixel object, e.g. pixels.
- speed: The refresh rate of the rainbow in seconds, e.g. 0.1.
Optional:
- size: The number of pixels to turn on in a row, e.g. 3. Defaults to 2 if no size is provided.
- spacing: The number of pixels to turn off in a row, e.g. 6. Defaults to 3 if no size is provided.
- reverse: Optionally reverses the movement of the animation. Set to True to enable. Defaults to False.
- step: The steps to take through the colorwheel (0-255). A step of 1 means cycling through the entire colorwheel, a step of 2 means it cycles through every other possible value. Defaults to 8 if no step is provided.
Once created, you display the animation.
Download: file
rainbow_chase = RainbowChase(pixels, speed=0.1, size=5, spacing=3)
while True:
rainbow_chase.animate()
That's all there is to displaying a rainbow theatre chase animation using the LED Animation library! Let's take a look at the next animation.
RainbowComet
This is a rainbow version of a comet of a specified speed, with a dimming tail of specified length.
First, you import the RainbowComet module. See Import and Setup for the rest of the necessary imports and pixel object creation.
Download: file
from adafruit_led_animation.animation.rainbowcomet import RainbowComet
Next you create the RainbowComet animation. RainbowComet requires two arguments and has an optional four more. You'll likely want to specify at least tail_length.
Required:
- pixel_object: The pixel object, e.g. pixels.
- speed: The speed of the comet in seconds, e.g. 0.1.
Optional:
- tail_length: The length of the comet in pixels. Defaults to 25% of the length of the pixel_object if no length is provided. Automatically compensates for a minimum length of 2 and a maximum of the length of the pixel_object.
- reverse: Optionally reverses the movement of the animation. Set to True to enable. Defaults to False.
- bounce: Optionally "bounces" the comet along the strip by displaying it from the beginning of the strip to the end, and then reversing the movement once it reaches the end of the strip. Set to True to enable. Defaults to False.
- colorwheel_offset: Offset from the start of the colorwheel. Provide a value of 0-255 where 0 is red, 85 is blue and 170 is green, wrapping back to 255 being red. Defaults to 0.
Once created, you display the animation.
Download: file
rainbow_comet = RainbowComet(pixels, speed=0.1, tail_length=7, bounce=True)
while True:
rainbow_comet.animate()
RainbowSparkle
This is a shifting rainbow that sparkles.
First, you import the RainbowSparkle module. See Import and Setup for the rest of the necessary imports and pixel object creation.
Download: file
from adafruit_led_animation.animation.rainbowsparkle import RainbowSparkle
Next you create the RainbowSparkle animation. RainbowSparkle requires two arguments and has an optional five more.
Required:
- pixel_object: The pixel object, e.g. pixels.
- speed: The refresh rate of the rainbow in seconds, e.g. 0.1.
Optional:
- period: The period over which to cycle the rainbow in seconds, e.g. 2. Defaults to 5 if no period is provided.
- num_sparkles: The number of sparkles. Defaults to 5% of the length of the pixel_object.
- step: The steps to take through the colorwheel (0-255). A step of 1 means cycling through the entire colorwheel, a step of 2 means it cycles through every other possible value. Defaults to 1 if no step is provided.
- precompute_rainbow: Precompute the rainbow which increases its speed but uses more memory. Set to False to disable if you are running into memory limitations. Defaults to True.
Once created, you display the animation.
Download: file
rainbow_sparkle = RainbowSparkle(pixels, speed=0.1, num_sparkles=15)
while True:
rainbow_sparkle.animate()
That's how to display a rainbow sparkle animation using the LED Animation library! Next up: sparkles!
Full Example Code
This example runs all the rainbow animations in sequence.
Download: Project Zip or led_animation_rainbow_animations.py | View on Github
"""
This example uses AnimationsSequence to display multiple animations in sequence, at a five second
interval.
For NeoPixel FeatherWing. Update pixel_pin and pixel_num to match your wiring if using
a different form of NeoPixels.
This example does not work on SAMD21 (M0) boards.
"""
import board
import neopixel
from adafruit_led_animation.animation.rainbow import Rainbow
from adafruit_led_animation.animation.rainbowchase import RainbowChase
from adafruit_led_animation.animation.rainbowcomet import RainbowComet
from adafruit_led_animation.animation.rainbowsparkle import RainbowSparkle
from adafruit_led_animation.sequence import AnimationSequence
# Update to match the pin connected to your NeoPixels
pixel_pin = board.D6
# Update to match the number of NeoPixels you have connected
pixel_num = 32
pixels = neopixel.NeoPixel(pixel_pin, pixel_num, brightness=0.5, auto_write=False)
rainbow = Rainbow(pixels, speed=0.1, period=2)
rainbow_chase = RainbowChase(pixels, speed=0.1, size=5, spacing=3)
rainbow_comet = RainbowComet(pixels, speed=0.1, tail_length=7, bounce=True)
rainbow_sparkle = RainbowSparkle(pixels, speed=0.1, num_sparkles=15)
animations = AnimationSequence(
rainbow,
rainbow_chase,
rainbow_comet,
rainbow_sparkle,
advance_interval=5,
auto_clear=True,
)
while True:
animations.animate()
Sparkle
The CircuitPython LED Animation library includes a series of sparkle animations: sparkle and sparklepulse. This section will cover these animations and the available customizations for each of them.
Most animations will run individually on the SAMD21 (M0) microcontroller boards, but some combinations of animations and the most complex animations will not. If you're interested in running all the animations, or many animations together, consider using at least a SAMD51 (M4) microcontroller.
Sparkle
This animation sparkles across all of the pixels in a single color.
First, you import the Sparkle module and a color for it. See Import and Setup for the rest of the necessary imports and pixel object creation.
Download: file
from adafruit_led_animation.animation.sparkle import Sparkle
from adafruit_led_animation.color import AMBER
Next you create the Sparkle animation. Sparkle requires two arguments and has an optional third.
Required:
- pixel_object: The pixel object, e.g. pixels.
- speed: The refresh rate of the rainbow in seconds, e.g. 0.05.
- color: The color to display, e.g. AMBER. Can also be a color tuple, e.g. (255, 0, 0), or a hex color value, e.g. 0xFF0000.
Optional:
- num_sparkles: The number of sparkles. Defaults to 5% of the length of the pixel_object.
Once created, you display the animation.
Download: file
sparkle = Sparkle(pixels, speed=0.05, color=AMBER, num_sparkles=10)
while True:
sparkle.animate()
SparklePulse
This is a version of sparkle that uses pulse to determine the brightness of each pixel.
First, you import the SparklePulse module and a color for it. See Import and Setup for the rest of the necessary imports and pixel object creation.
Download: file
sparkle_pulse = SparklePulse(pixels, speed=0.05, period=3, color=JADE)
from adafruit_led_animation.color import JADE
Next you create the SparklePulse animation. SparklePulse requires three arguments and has an optional three more.
Required:
- pixel_object: The pixel object, e.g. pixels.
- speed: The speed of the pulse in seconds, e.g. 0.05.
- color: The color to display, e.g. JADE. Can also be a color tuple, e.g. (255, 0, 0), or a hex color value, e.g. 0xFF0000.
Optional:
- period: The number of seconds over which to pulse the LEDs. Defaults to 5 if no period is provided.
- max_intensity: The maximum intensity to pulse. Provide a value between 0 and 1.0. Defaults to 1.
- min_intensity: The minimum intensity to pulse. Provide a value between 0 and 1.0. Defaults to 0.
Once created, you display the animation.
Download: file
sparkle_pulse = SparklePulse(pixels, speed=0.05, period=3, color=JADE)
while True:
sparkle_pulse.animate()
Next, we'll look at using the pixel mapping helpers to create a grid from a single LED strip.
Full Example Code
This example displays the sparkle animations in sequence.
Download: Project Zip or led_animation_sparkle_animations.py | View on Github
"""
This example uses AnimationsSequence to display multiple animations in sequence, at a five second
interval.
For NeoPixel FeatherWing. Update pixel_pin and pixel_num to match your wiring if using
a different form of NeoPixels.
"""
import board
import neopixel
from adafruit_led_animation.animation.sparkle import Sparkle
from adafruit_led_animation.animation.sparklepulse import SparklePulse
from adafruit_led_animation.sequence import AnimationSequence
from adafruit_led_animation.color import AMBER, JADE
# Update to match the pin connected to your NeoPixels
pixel_pin = board.D6
# Update to match the number of NeoPixels you have connected
pixel_num = 32
pixels = neopixel.NeoPixel(pixel_pin, pixel_num, brightness=0.5, auto_write=False)
sparkle = Sparkle(pixels, speed=0.05, color=AMBER, num_sparkles=10)
sparkle_pulse = SparklePulse(pixels, speed=0.05, period=3, color=JADE)
animations = AnimationSequence(
sparkle, sparkle_pulse, advance_interval=5, auto_clear=True,
)
while True:
animations.animate()
Pixel Mapping
The CircuitPython LED Animation library includes pixel mapping helpers to make it super simple to treat a single LED strip as a grid. This is handy when you are using an LED matrix that is essentially one strip in series, or if you have a series of strips arranged in a grid. This section will go over the basics of the pixel mapping feature of the library and show you how to use it with animations.
Most animations will run individually on the SAMD21 (M0) microcontroller boards, but some combinations of animations, the most complex animations, and complex pixel mapping will not. If you're interested in running all the animations, many animations together, or a complex pixel map, consider using at least a SAMD51 (M4) microcontroller.
LED Matrices
Many LED matrices look like a matrix at first glance, but they're actually a strip of pixels arranged as a grid. The NeoPixel FeatherWing is a set of NeoPixels made up of 32 pixels that are arranged in an 8x4 pixel grid. It's arranged left to right, beginning in the upper left corner near the "NeoPixel FeatherWing" silk print, and ending in the bottom left near the DOUT pin, with each row beginning on the left and ending on the right.
If you want to see the pixel arrangement, try animating a comet with the initial pixel object. It will follow the pixel "strip". But what if you want to treat it as a matrix to display animations across it horizontally or vertically? PixelMap has helpers to do exactly that.
PixelMap
The PixelMap helper enables you to treat a strip or strips of LEDs as a grid for animation purposes. It also works great with LED matrices that are actually a strip of LEDs arranged in a matrix, such as the NeoPixel FeatherWing. The example on this page uses the NeoPixel FeatherWing but should be quick to adapt to any grid or matrix.
First, you'll need to import the helper module. You'll also import the other required libraries, a number of animations and colors for some of them, and AnimationSequence.
Download: file
import board
import neopixel
from adafruit_led_animation.animation.comet import Comet
from adafruit_led_animation.animation.rainbowcomet import RainbowComet
from adafruit_led_animation.animation.rainbowchase import RainbowChase
from adafruit_led_animation.animation.chase import Chase
from adafruit_led_animation.animation.rainbow import Rainbow
from adafruit_led_animation.sequence import AnimationSequence
from adafruit_led_animation import helper
from adafruit_led_animation.color import PURPLE, JADE, AMBER
Next you create the initial pixel object. This is identical to the pixel object used in all the previous examples - it sets up the pixels for use by the code.
If you're using some other NeoPixel form factor, update pixel_pin and pixel_num to match your NeoPixel setup. However, be aware that this example is designed for 32 pixels in an 8x4 matrix, and will require other changes to run properly if using a different setup.
Download: file
pixel_pin = board.D6
pixel_num = 32
pixels = neopixel.NeoPixel(pixel_pin, pixel_num, brightness=0.2, auto_write=False)
Next, you're going to create two new pixel objects using the PixelMap and horizontal_strip_gridmap helpers. One will be to create grid on which to animate vertically, and the other to animate horizontally.
PixelMap has two grid options for creating a grid: vertical_lines and horizontal_lines. The first generates a pixel map of vertical lines on a strip arranged in a grid, and the second generates a pixel map of horizontal lines on a strip arranged in a grid. Both of these helpers have four required arguments.
- pixel_object: The initial pixel object, e.g. pixels.
- width: The width of the grid, e.g. 8.
- height: The height of the grid, e.g. 4.
- gridmap: A function to map x and y coordinates to the grid, e.g. horizontal_strip_gridmap or vertical_strip_gridmap.
As the NeoPixel FeatherWing is arranged horizontally, you'll be using the horizontal_strip_gridmap helper. It has one required argument and one optional argument.
Required:
- width: The grid width in pixels, e.g. 8.
Optional:
- alternating: Whether or not the lines in the grid are running alternating directions in a zigzag. Defaults to True.
The NeoPixel FeatherWing lines do not run in alternating directions.
Download: file
pixel_wing_vertical = helper.PixelMap.vertical_lines(
pixels, 8, 4, helper.horizontal_strip_gridmap(8, alternating=False)
)
pixel_wing_horizontal = helper.PixelMap.horizontal_lines(
pixels, 8, 4, helper.horizontal_strip_gridmap(8, alternating=False)
)
Now that you've created these pixel objects, you can use them with the animations, the same way you used the initial pixel object.
To create a purple comet that is the width of the grid and animates top to bottom, you would create a comet animation as follows:
Download: file
comet_h = Comet(
pixel_wing_horizontal, speed=0.1, color=PURPLE, tail_length=3, bounce=True
)
To create an amber comet that is the height of the grid and animates left to right, you would create a comet as follows:
Download: file
comet_v = Comet(pixel_wing_vertical, speed=0.1, color=AMBER, tail_length=6, bounce=True)
To create a jade chase animation that animates from top to bottom:
Download: file
chase_h = Chase(pixel_wing_horizontal, speed=0.1, size=3, spacing=6, color=JADE)
To create a rainbow chase animation that animates from left to right:
Download: file
rainbow_chase_v = RainbowChase(
pixel_wing_vertical, speed=0.1, size=3, spacing=2, wheel_step=8
)
To create a rainbow comet that animates across the grid from left to right:
Download: file
rainbow_comet_v = RainbowComet(
pixel_wing_vertical, speed=0.1, tail_length=7, bounce=True
)
To create a rainbow that cycles across the grid vertically:
Download: file
rainbow_v = Rainbow(pixel_wing_vertical, speed=0.1, period=2)
And finally, to create a rainbow chase that animates from top to bottom:
Download: file
rainbow_chase_h = RainbowChase(pixel_wing_horizontal, speed=0.1, size=3, spacing=3)
Then you would display these animations the same way you did previously.
Download: file
animations = AnimationSequence(
rainbow_v,
comet_h,
rainbow_comet_v,
chase_h,
rainbow_chase_v,
comet_v,
rainbow_chase_h,
advance_interval=5,
)
while True:
animations.animate()
The same follows for any other animation. Some animations do not make sense to use with these helpers like blink, colorcycle, sparkle and pulse, as they use all the LEDs and the arrangement is irrelevant.
Now you can create animations that display horizontally and vertically across a grid!
Full Example Code
This example displays five different animations horizontally and vertically across a grid.
Download: Project Zip or led_animation_pixel_map.py | View on Github
"""
This example shows usage of the PixelMap helper to easily treat a single strip as a horizontal or
vertical grid for animation purposes.
For NeoPixel FeatherWing. Update pixel_pin and pixel_num to match your wiring if using
a different form of NeoPixels. Note that if you are using a number of pixels other than 32, you
will need to alter the PixelMap values as well for this example to work.
This example does not work on SAMD21 (M0) boards.
"""
import board
import neopixel
from adafruit_led_animation.animation.comet import Comet
from adafruit_led_animation.animation.rainbowcomet import RainbowComet
from adafruit_led_animation.animation.rainbowchase import RainbowChase
from adafruit_led_animation.animation.chase import Chase
from adafruit_led_animation.animation.rainbow import Rainbow
from adafruit_led_animation.sequence import AnimationSequence
from adafruit_led_animation import helper
from adafruit_led_animation.color import PURPLE, JADE, AMBER
# Update to match the pin connected to your NeoPixels
pixel_pin = board.D6
# Update to match the number of NeoPixels you have connected
pixel_num = 32
pixels = neopixel.NeoPixel(pixel_pin, pixel_num, brightness=0.5, auto_write=False)
pixel_wing_vertical = helper.PixelMap.vertical_lines(
pixels, 8, 4, helper.horizontal_strip_gridmap(8, alternating=False)
)
pixel_wing_horizontal = helper.PixelMap.horizontal_lines(
pixels, 8, 4, helper.horizontal_strip_gridmap(8, alternating=False)
)
comet_h = Comet(
pixel_wing_horizontal, speed=0.1, color=PURPLE, tail_length=3, bounce=True
)
comet_v = Comet(pixel_wing_vertical, speed=0.1, color=AMBER, tail_length=6, bounce=True)
chase_h = Chase(pixel_wing_horizontal, speed=0.1, size=3, spacing=6, color=JADE)
rainbow_chase_v = RainbowChase(
pixel_wing_vertical, speed=0.1, size=3, spacing=2, step=8
)
rainbow_comet_v = RainbowComet(
pixel_wing_vertical, speed=0.1, tail_length=7, bounce=True
)
rainbow_v = Rainbow(pixel_wing_vertical, speed=0.1, period=2)
rainbow_chase_h = RainbowChase(pixel_wing_horizontal, speed=0.1, size=3, spacing=3)
animations = AnimationSequence(
rainbow_v,
comet_h,
rainbow_comet_v,
chase_h,
rainbow_chase_v,
comet_v,
rainbow_chase_h,
advance_interval=5,
)
while True:
animations.animate()
Animation Group
The CircuitPython LED Animation library includes an animation group helper that enables you to synchronize groups of animations. This section will walk through the basics of the animation group feature of the library and show you how to use it with animations and pixel objects.
Most animations will run individually on the SAMD21 (M0) microcontroller boards, but some combinations of animations, the most complex animations, and animation groups will not. If you're interested in running all the animations, many animations together, or an animation group, consider using at least a SAMD51 (M4) microcontroller.
AnimationGroup
The AnimationGroup helper enables you to keep multiple animations in sync, whether or not the same animation or pixel object is used. It can be used with multiple animations or pixel objects, including pixel subsets. The example on this page is written for Circuit Playground Bluefruit and a 30-pixel NeoPixel LED strip, connected to pad A1.
First, you'll need to import the AnimationGroup module. You'll also import the other required libraries, the CircuitPlayground library, a number of animations and colors for them, and AnimationSequence.
Download: file
import board
import neopixel
from adafruit_circuitplayground import cp
from adafruit_led_animation.animation.blink import Blink
from adafruit_led_animation.animation.comet import Comet
from adafruit_led_animation.animation.chase import Chase
from adafruit_led_animation.group import AnimationGroup
from adafruit_led_animation.sequence import AnimationSequence
import adafruit_led_animation.color as color
Next, you'll create the pixel object for the strip, and specifically set the brightness for the Circuit Playground Bluefruit NeoPixels to 0.5.
Download: file
strip_pixels = neopixel.NeoPixel(board.A1, 30, brightness=0.5, auto_write=False)
cp.pixels.brightness = 0.5
Then you create an animation sequence. But this time, instead of simply adding animations, you're also going to add animation groups.
The first group is made up of the same animation on both the CPB and the strip, but we'll set each animation to a different speed. Then, we'll set sync=True. This means that when the animations are displayed, the different speed of the second animation is ignored, and the speed of the two animations is synced to the speed specified in the first one.
Download: file
animations = AnimationSequence(
AnimationGroup(
Blink(cp.pixels, 0.5, color.CYAN),
Blink(strip_pixels, 3.0, color.AMBER),
sync=True,
),
The second group is also made up of the same animation on both, and we set each one to a different speed. This time, we won't sync them.
Download: file
[...] # Means there's code above here in this code block.
AnimationGroup(
Comet(cp.pixels, 0.1, color.MAGENTA, tail_length=5),
Comet(strip_pixels, 0.01, color.MAGENTA, tail_length=15),
),
The third group is made up of two different animations, one on the CPB and one on the strip. It displays two different animations on two different pixel objects simultaneously.
Download: file
[...]
AnimationGroup(
Blink(cp.pixels, 0.5, color.JADE),
Comet(strip_pixels, 0.05, color.TEAL, tail_length=15),
),
And finally, you include two animations in the sequence that will display sequentially, first on the CPB and then on the strip.
The advance interval is set to 3 seconds, and auto_clear and auto_reset are set to True.
Download: file
[...]
Chase(cp.pixels, 0.05, size=2, spacing=3, color=color.PURPLE),
Chase(strip_pixels, 0.05, size=2, spacing=3, color=color.PURPLE),
advance_interval=3.0,
auto_clear=True,
auto_reset=True,
)
You display the animations the same way you have in the previous sections.
Download: file
while True:
animations.animate()
That's all there is to using AnimationGroup to display and synchronise groups of animations using the LED Animation library!
Full Example Code
This example uses animation groups to display multiple animations simultaneously.
Download: Project Zip or led_animation_group.py | View on Github
"""
This example shows three different ways to use AnimationGroup: syncing two animations, displaying
two animations at different speeds, and displaying two animations sequentially, across two separate
pixel objects such as the built-in NeoPixels on a Circuit Playground Bluefruit and a NeoPixel strip.
This example is written for Circuit Playground Bluefruit and a 30-pixel NeoPixel strip connected to
pad A1. It does not work on Circuit Playground Express.
"""
import board
import neopixel
from adafruit_circuitplayground import cp
from adafruit_led_animation.animation.blink import Blink
from adafruit_led_animation.animation.comet import Comet
from adafruit_led_animation.animation.chase import Chase
from adafruit_led_animation.group import AnimationGroup
from adafruit_led_animation.sequence import AnimationSequence
import adafruit_led_animation.color as color
strip_pixels = neopixel.NeoPixel(board.A1, 30, brightness=0.5, auto_write=False)
cp.pixels.brightness = 0.5
animations = AnimationSequence(
# Synchronized to 0.5 seconds. Ignores the second animation setting of 3 seconds.
AnimationGroup(
Blink(cp.pixels, 0.5, color.CYAN),
Blink(strip_pixels, 3.0, color.AMBER),
sync=True,
),
# Different speeds
AnimationGroup(
Comet(cp.pixels, 0.1, color.MAGENTA, tail_length=5),
Comet(strip_pixels, 0.01, color.MAGENTA, tail_length=15),
),
# Different animations
AnimationGroup(
Blink(cp.pixels, 0.5, color.JADE),
Comet(strip_pixels, 0.05, color.TEAL, tail_length=15),
),
# Sequential animations on the built-in NeoPixels then the NeoPixel strip
Chase(cp.pixels, 0.05, size=2, spacing=3, color=color.PURPLE),
Chase(strip_pixels, 0.05, size=2, spacing=3, color=color.PURPLE),
advance_interval=3.0,
auto_clear=True,
auto_reset=True,
)
while True:
animations.animate()