Shown here is an example of the documents section. The user manuals, data sheets, and application notes are all here. Efinix has several application notes on the MIPI demos, including a spreadsheet utility to help the customer configure the MIPI interface. These documents are important to read if the customer is planning on using the MIPI/CSI hard blocks. All this data is open to any user to see, as there is no password required. Access to this information is available under the support button in the upper right on Efinix Inc Web page, navigate there and then hit documentation.