These two windows explain the assembly order of UniMEC™ accessories. The LEDs and lenses are pushed into the bezel and are added to the switch simultaneously. It is important with the alternate version that the actuator is in the upper position when dismounting the accessories, as well as during soldering in order to keep the functionality of the switch. As mentioned earlier, UniMEC has 8 contact functions which can be seen in the wiring diagram.